I'm trying to use the LCr to display several thousand images, as fast as possible. As of the 2.0.1 update, I see that there is an option for using the HDMI input mode to re-interpret a 24-bit HDMI signal as 24 1-bit images, thus improving the frame rate. My current video card (GeForce GT520) only supports 8-, 16-, and 32- bits-per-pixel (bbp) color palette. Does the video card specifically need to support 24-bit color or can I use the 32-bbp mode? Also, how does the output trigger look like when in HDMI mode? Will it give a 60 Hz signal or 24 * 60 Hz?
Thanks!