Hello community menbers.
I'm working in an application that requires the projection of a large number of light patterns at a very high speed.
From the data manual of the 0.55XGA Chipset : "... enables DMD patterns to be refreshed with frequency rates up to 5000Hz binary and over 700 Hz in 8 bit Gray scale." .
- I would like to know how to determine the maximum bit depth at a specific frame rate, since the application works between the 700 and 5000 hz limits and requires the highest possible bit depth.
 
I'm also interested in expanding the 960 binary patterns limit of the chipset. From the data manual: "The 0.55 XGA Chipset relies on the use of SDRAM to store DMD formatted patterns."
- Which is this format?
 - What is the size of a XGA 8 bit depth image in this format?
 - Is the amount of memory that can be addressed by the DLPC 200 SDRAM INTERFACE the limitation?
 - Are there other limitations?
 
Regards.
Enio