This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
First of all, thanks for assisting me with this issue.
I'm using the BQ 25504 to harvest power from a photovoltaic array to charge a battery. I've built the typical solar cell application circuit as described in the data sheet. I'm currently using a photodiode array (in a combination of series and parallel configuration) to act as my solar cells. Instead of a battery, I have a 300uF capacity in parallel with a variable resistor (resistor decade box). So the variable resistor is connected to the PIN 14 VBAT and the 300uF capacitor is attached to VSTOR PIN 15. I'm using this variable resistor to measure maximum power output from the chip's circuit.
At low light intensities (incident on the photodiode array), the MPPT works as it should and the voltage across the photodiodes is around 0.8V (Voc of around 1V). However, as I increase my light intensity, the MPPT stops functioning and the the voltage across the solar cells goes to >90% of Voc.
The MPPT also stops functioning as i increase the resistance on the variable resistor.
Why doesn't the MPPT always hold the voltage across the photodiode array at the desired 79%.
Assuming your panel's VOC < VBAT_OV setting, as the power output capability of the solar panel increases (i.e., its output impedance goes down), the hysteretic boost power FET, pulling only up to 200mA from the panel, can't pull enough current to discharge the input capacitor to the MPP. This means that the IC is pulling all of the power it can from the panel even though the panel can provide more power, even though it is technically not at its MPP.
If VOC > VBAT_OV and VSTOR = VBAT_OV then the IC has a pull down resistor on VIN_DC that pulls the VIN_DC to down VSTOR.
I can't explain why increasing what I assume is a variable resistor in series with the panel causes the MPP to stop functioning unless you have increased it so high that the IC can't get enough power to keep VSTOR > 1.8V.