This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I recently bought a XDS100v2 (Blackhawk, Model D) and downloaded the CCS V5 (meanwhile with latest updates installed).
I've a custom board with two DSPs in a chain (hardware out of doubt as full functioning with CCS V3.3 and a BH560 emulator) were the JTAG chain is o.k. (as assumed by CCS V5 & XDS100v2).
I can connect to the first DSP in the chain, download a program and run it !
Unfortunately when I try to connect the second CPU the hole CCS crashes without any error message.
Has someone an Idea where to start.
Regards, Wolfgang
Are there any crash dump logs created? (see here ). If there are, would you be able to attach them to this thread?
If there are not crash dump logs, it would be useful to get a Debug Server log from the debug session where CCS crashes. That is described in the same wiki topic.
# # An unexpected error has been detected by Java Runtime Environment: # # EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x3a81c2df, pid=5920, tid=5644 # # Java VM: Java HotSpot(TM) Client VM (11.3-b02 mixed mode windows-x86) # Problematic frame: # C 0x3a81c2df # # If you would like to submit a bug report, please visit: # http://java.sun.com/webapps/bugreport/crash.jsp # The crash happened outside the Java Virtual Machine in native code. # See problematic frame for where to report the bug. # --------------- T H R E A D --------------- Current thread (0x2e038400): JavaThread "polling thread" daemon [_thread_in_native, id=5644, stack(0x36bc0000,0x36cc0000)] siginfo: ExceptionCode=0xc0000005, reading address 0x00000000 Registers: EAX=0x00000000, EBX=0x2fc33501, ECX=0x00000000, EDX=0x00000008 ESP=0x36cbf308, EBP=0x36cbf538, ESI=0x3033b340, EDI=0x10000000 EIP=0x3a81c2df, EFLAGS=0x00010202 Top of Stack: (sp=0x36cbf308) 0x36cbf308: 00000000 2fc33570 302a9ce0 00000000 0x36cbf318: 3a7eec9f 3033b301 302adfe8 3a7f1d0e 0x36cbf328: 302a9b70 00000000 302adfe8 fffffc14 0x36cbf338: 00000200 00000000 302adfe8 2fc33570 0x36cbf348: 3aa20020 00000000 00000024 00000001 0x36cbf358: 00000000 00000000 00000000 00000000 0x36cbf368: 00000000 00000000 00000000 00000da8 0x36cbf378: 00000710 013e0001 00000083 3a609520 Instructions: (pc=0x3a81c2df) 0x3a81c2cf: 59 c3 84 db 74 1f 8b 46 0c 8b 4c 24 0c 8d 50 08 0x3a81c2df: 8b 00 52 8b 56 28 50 51 52 e8 93 20 00 00 83 c4 Stack: [0x36bc0000,0x36cc0000], sp=0x36cbf308, free space=1020k Native frames: (J=compiled Java code, j=interpreted, Vv=VM code, C=native code) C 0x3a81c2df Java frames: (J=compiled Java code, j=interpreted, Vv=VM code) j com.ti.xpcom.internal.XPCOMJavaProxy.callXPCOMMethod(JLjava/lang/String;[Ljava/lang/Object;)Ljava/lang/Object;+0 j com.ti.xpcom.internal.XPCOMJavaProxy.invoke(Ljava/lang/Object;Ljava/lang/reflect/Method;[Ljava/lang/Object;)Ljava/lang/Object;+104 j $Proxy2.pollThreadMain()J+9 j com.ti.debug.engine.cce.CCEDebugEngine.pollThreadMain()J+7 j com.ti.debug.engine.cce.CCEDebugEngine$PollingThread.run()V+122 v ~StubRoutines::call_stub --------------- P R O C E S S --------------- Java Threads: ( => current thread ) 0x31136800 JavaThread "SystemAnalyzer.stringQueue" [_thread_blocked, id=5436, stack(0x3b190000,0x3b290000)] 0x2e03a400 JavaThread "Worker-10" [_thread_blocked, id=2340, stack(0x39fd0000,0x3a0d0000)] 0x2e03c400 JavaThread "com.ti.ccstudio.debug.debugModel - 0" [_thread_blocked, id=6048, stack(0x3a360000,0x3a460000)] 0x2e03bc00 JavaThread "Keep-Alive-Timer" daemon [_thread_blocked, id=528, stack(0x3a260000,0x3a360000)] 0x2e03a000 JavaThread "Worker-9" [_thread_blocked, id=5756, stack(0x37e90000,0x37f90000)] 0x2e039400 JavaThread "org.eclipse.cdt.internal.ui.text.CReconciler" daemon [_thread_blocked, id=1408, stack(0x37d50000,0x37e50000)] 0x2e038800 JavaThread "Worker-8" [_thread_blocked, id=4292, stack(0x37960000,0x37a60000)] 0x2e039000 JavaThread "org.eclipse.cdt.internal.ui.text.CReconciler" daemon [_thread_blocked, id=6068, stack(0x37ae0000,0x37be0000)] =>0x2e038400 JavaThread "polling thread" daemon [_thread_in_native, id=5644, stack(0x36bc0000,0x36cc0000)] 0x2e036000 JavaThread "Scripting Console - Rhino" [_thread_blocked, id=4720, stack(0x362f0000,0x363f0000)] 0x2e037800 JavaThread "Worker-7" [_thread_blocked, id=5352, stack(0x34700000,0x34800000)] 0x2e037000 JavaThread "Worker-6" [_thread_blocked, id=4396, stack(0x345c0000,0x346c0000)] 0x2e035c00 JavaThread "Worker-5" [_thread_blocked, id=2908, stack(0x34480000,0x34580000)] 0x2e035400 JavaThread "Worker-4" [_thread_blocked, id=4820, stack(0x30bf0000,0x30cf0000)] 0x2e034800 JavaThread "Worker-3" [_thread_blocked, id=5676, stack(0x2f610000,0x2f710000)] 0x2e036c00 JavaThread "org.eclipse.jface.text.reconciler.MonoReconciler" daemon [_thread_blocked, id=5236, stack(0x2f770000,0x2f870000)] 0x2e035000 JavaThread "Bundle File Closer" daemon [_thread_blocked, id=5988, stack(0x2dc60000,0x2dd60000)] 0x2e1bdc00 JavaThread "Worker-2" [_thread_blocked, id=5820, stack(0x2ed10000,0x2ee10000)] 0x2e1a3000 JavaThread "Worker-1" [_thread_blocked, id=2004, stack(0x2ec10000,0x2ed10000)] 0x2e069800 JavaThread "Worker-0" [_thread_blocked, id=5932, stack(0x2eb10000,0x2ec10000)] 0x2df3f800 JavaThread "Worker-JM" [_thread_blocked, id=2676, stack(0x2e350000,0x2e450000)] 0x2d2d5c00 JavaThread "[Timer] - Main Queue Handler" daemon [_thread_blocked, id=4232, stack(0x2dd60000,0x2de60000)] 0x2d276c00 JavaThread "Framework Event Dispatcher" daemon [_thread_blocked, id=3012, stack(0x2db60000,0x2dc60000)] 0x2d20ec00 JavaThread "Start Level Event Dispatcher" daemon [_thread_blocked, id=5940, stack(0x2da60000,0x2db60000)] 0x2d20dc00 JavaThread "State Data Manager" daemon [_thread_blocked, id=2492, stack(0x2d960000,0x2da60000)] 0x2d1ed800 JavaThread "Framework Active Thread" [_thread_blocked, id=1044, stack(0x2d860000,0x2d960000)] 0x025db000 JavaThread "Low Memory Detector" daemon [_thread_blocked, id=5848, stack(0x2cec0000,0x2cfc0000)] 0x025d6c00 JavaThread "CompilerThread0" daemon [_thread_blocked, id=4748, stack(0x2cdc0000,0x2cec0000)] 0x025d4400 JavaThread "Attach Listener" daemon [_thread_blocked, id=3244, stack(0x2ccc0000,0x2cdc0000)] 0x025c9c00 JavaThread "Signal Dispatcher" daemon [_thread_blocked, id=4572, stack(0x2cbc0000,0x2ccc0000)] 0x025b5400 JavaThread "Finalizer" daemon [_thread_blocked, id=2368, stack(0x2cac0000,0x2cbc0000)] 0x025b4000 JavaThread "Reference Handler" daemon [_thread_blocked, id=948, stack(0x2c9c0000,0x2cac0000)] 0x026a9c00 JavaThread "main" [_thread_in_native, id=4768, stack(0x00090000,0x00190000)] Other Threads: 0x025ae400 VMThread [stack: 0x2c8c0000,0x2c9c0000] [id=2456] 0x025e4000 WatcherThread [stack: 0x2d000000,0x2d100000] [id=1152] VM state:not at safepoint (normal execution) VM Mutex/Monitor currently owned by a thread: None Heap def new generation total 11136K, used 8547K [0x046b0000, 0x052c0000, 0x06430000) eden space 9920K, 78% used [0x046b0000, 0x04e44a68, 0x05060000) from space 1216K, 64% used [0x05060000, 0x05124390, 0x05190000) to space 1216K, 0% used [0x05190000, 0x05190000, 0x052c0000) tenured generation total 146844K, used 99507K [0x06430000, 0x0f397000, 0x1c6b0000) the space 146844K, 67% used [0x06430000, 0x0c55cee0, 0x0c55d000, 0x0f397000) compacting perm gen total 75264K, used 75150K [0x1c6b0000, 0x21030000, 0x2c6b0000) the space 75264K, 99% used [0x1c6b0000, 0x21013b00, 0x21013c00, 0x21030000) No shared spaces configured. Dynamic libraries: 0x00400000 - 0x0040d000 C:\CDs\ccsv5\eclipse\ccstudio.exe 0x77900000 - 0x77a80000 C:\Windows\SysWOW64\ntdll.dll 0x76ef0000 - 0x77000000 C:\Windows\syswow64\kernel32.dll 0x76430000 - 0x76477000 C:\Windows\syswow64\KERNELBASE.dll 0x76c30000 - 0x76d30000 C:\Windows\syswow64\USER32.dll 0x75570000 - 0x75600000 C:\Windows\syswow64\GDI32.dll 0x75330000 - 0x7533a000 C:\Windows\syswow64\LPK.dll 0x75740000 - 0x757dd000 C:\Windows\syswow64\USP10.dll 0x76dc0000 - 0x76e6c000 C:\Windows\syswow64\msvcrt.dll 0x76480000 - 0x76520000 C:\Windows\syswow64\ADVAPI32.dll 0x76520000 - 0x76539000 C:\Windows\SysWOW64\sechost.dll 0x768c0000 - 0x769b0000 C:\Windows\syswow64\RPCRT4.dll 0x74fe0000 - 0x75040000 C:\Windows\syswow64\SspiCli.dll 0x74fd0000 - 0x74fdc000 C:\Windows\syswow64\CRYPTBASE.dll 0x741b0000 - 0x74234000 C:\Windows\WinSxS\x86_microsoft.windows.common-controls_6595b64144ccf1df_5.82.7601.17514_none_ec83dffa859149af\COMCTL32.dll 0x71610000 - 0x7165c000 C:\Windows\system32\apphelp.dll 0x72ed0000 - 0x72f5d000 C:\Windows\AppPatch\AcLayers.DLL 0x757e0000 - 0x7642a000 C:\Windows\syswow64\SHELL32.dll 0x75690000 - 0x756e7000 C:\Windows\syswow64\SHLWAPI.dll 0x76ad0000 - 0x76c2c000 C:\Windows\syswow64\ole32.dll 0x76540000 - 0x765cf000 C:\Windows\syswow64\OLEAUT32.dll 0x73400000 - 0x73417000 C:\Windows\system32\USERENV.dll 0x745e0000 - 0x745eb000 C:\Windows\system32\profapi.dll 0x74ea0000 - 0x74ef1000 C:\Windows\system32\WINSPOOL.DRV 0x74990000 - 0x749a2000 C:\Windows\system32\MPR.dll 0x76740000 - 0x767a0000 C:\Windows\system32\IMM32.DLL 0x75240000 - 0x7530c000 C:\Windows\syswow64\MSCTF.dll 0x72000000 - 0x7200d000 C:\CDs\ccsv5\eclipse\plugins\org.eclipse.equinox.launcher.win32.win32.x86_1.1.200.v20120522-1813\eclipse_1503.dll 0x74f00000 - 0x74f09000 C:\Windows\system32\VERSION.dll 0x74690000 - 0x74710000 C:\Windows\system32\uxtheme.dll 0x71830000 - 0x718d1000 c:\Program Files (x86)\Hewlett-Packard\HP ProtectTools Security Manager\Bin\DpoFeedb.dll 0x75600000 - 0x75683000 C:\Windows\syswow64\CLBCatQ.DLL 0x6d800000 - 0x6da56000 C:\CDs\ccsv5\eclipse\jre\bin\client\jvm.dll 0x74740000 - 0x74772000 C:\Windows\system32\WINMM.dll 0x7c340000 - 0x7c396000 C:\Windows\system32\MSVCR71.dll 0x6d290000 - 0x6d298000 C:\CDs\ccsv5\eclipse\jre\bin\hpi.dll 0x75320000 - 0x75325000 C:\Windows\syswow64\PSAPI.DLL 0x6d7b0000 - 0x6d7bc000 C:\CDs\ccsv5\eclipse\jre\bin\verify.dll 0x6d330000 - 0x6d34f000 C:\CDs\ccsv5\eclipse\jre\bin\java.dll 0x6d7f0000 - 0x6d7ff000 C:\CDs\ccsv5\eclipse\jre\bin\zip.dll 0x74570000 - 0x74586000 C:\Windows\system32\CRYPTSP.dll 0x74530000 - 0x7456b000 C:\Windows\system32\rsaenh.dll 0x6d610000 - 0x6d623000 C:\CDs\ccsv5\eclipse\jre\bin\net.dll 0x77000000 - 0x77035000 C:\Windows\syswow64\WS2_32.dll 0x75040000 - 0x75046000 C:\Windows\syswow64\NSI.dll 0x745a0000 - 0x745dc000 C:\Windows\system32\mswsock.dll 0x74250000 - 0x74256000 C:\Windows\System32\wship6.dll 0x74510000 - 0x74520000 C:\Windows\system32\NLAapi.dll 0x74500000 - 0x74510000 C:\Windows\system32\napinsp.dll 0x744e0000 - 0x744f2000 C:\Windows\system32\pnrpnsp.dll 0x74490000 - 0x744d4000 C:\Windows\system32\DNSAPI.dll 0x74480000 - 0x74488000 C:\Windows\System32\winrnr.dll 0x74590000 - 0x74595000 C:\Windows\System32\wshtcpip.dll 0x74720000 - 0x7473c000 C:\Windows\system32\IPHLPAPI.DLL 0x74710000 - 0x74717000 C:\Windows\system32\WINNSI.DLL 0x74430000 - 0x74436000 C:\Windows\system32\rasadhlp.dll 0x74440000 - 0x74478000 C:\Windows\System32\fwpuclnt.dll 0x6d630000 - 0x6d639000 C:\CDs\ccsv5\eclipse\jre\bin\nio.dll 0x2e590000 - 0x2e600000 C:\CDs\ccsv5\eclipse\configuration\org.eclipse.osgi\bundles\667\1\.cp\swt-win32-3834.dll 0x76e70000 - 0x76eeb000 C:\Windows\syswow64\comdlg32.dll 0x747f0000 - 0x7498e000 C:\Windows\WinSxS\x86_microsoft.windows.common-controls_6595b64144ccf1df_6.0.7601.17514_none_41e6975e2bd6f2b2\COMCTL32.dll 0x769b0000 - 0x76acb000 C:\Windows\syswow64\WININET.dll 0x778d0000 - 0x778d3000 C:\Windows\syswow64\Normaliz.dll 0x75050000 - 0x75208000 C:\Windows\syswow64\iertutil.dll 0x76620000 - 0x76731000 C:\Windows\syswow64\urlmon.dll 0x767a0000 - 0x768be000 C:\Windows\syswow64\CRYPT32.dll 0x75310000 - 0x7531c000 C:\Windows\syswow64\MSASN1.dll 0x73470000 - 0x73483000 C:\Windows\system32\dwmapi.dll 0x73260000 - 0x73355000 C:\Windows\system32\propsys.dll 0x74130000 - 0x74139000 C:\Windows\system32\LINKINFO.dll 0x2d550000 - 0x2d56d000 C:\CDs\ccsv5\eclipse\configuration\org.eclipse.osgi\bundles\667\1\.cp\swt-gdip-win32-3834.dll 0x70fa0000 - 0x71130000 C:\Windows\WinSxS\x86_microsoft.windows.gdiplus_6595b64144ccf1df_1.1.7601.17825_none_72d273598668a06b\gdiplus.dll 0x706f0000 - 0x707eb000 C:\Windows\system32\WindowsCodecs.dll 0x02690000 - 0x0269e000 C:\CDs\ccsv5\eclipse\configuration\org.eclipse.osgi\bundles\87\2\.cp\os\win32\x86\localfile_1_0_0.dll 0x2e450000 - 0x2e458000 C:\CDs\ccsv5\eclipse\configuration\org.eclipse.osgi\bundles\92\2\.cp\os\win32\x86\win32refresh.dll 0x720d0000 - 0x72119000 c:\Program Files (x86)\Hewlett-Packard\HP ProtectTools Security Manager\Bin\DpoSet.dll 0x71d80000 - 0x71dbc000 C:\Windows\system32\oleacc.dll 0x6f9d0000 - 0x6fb3f000 C:\Windows\system32\explorerframe.dll 0x74100000 - 0x7412f000 C:\Windows\system32\DUser.dll 0x70830000 - 0x708e2000 C:\Windows\system32\DUI70.dll 0x74140000 - 0x7414f000 C:\CDs\ccsv5\eclipse\configuration\org.eclipse.osgi\bundles\90\2\.cp\jWinHttp-1.0.0.dll 0x73550000 - 0x735a8000 C:\Windows\system32\WINHTTP.dll 0x73500000 - 0x7354f000 C:\Windows\system32\webio.dll 0x74180000 - 0x7418d000 C:\Windows\system32\dhcpcsvc6.DLL 0x74150000 - 0x74162000 C:\Windows\system32\dhcpcsvc.DLL 0x73620000 - 0x73628000 C:\Windows\system32\credssp.dll 0x765f0000 - 0x76617000 C:\Windows\syswow64\CFGMGR32.dll 0x73450000 - 0x7345e000 C:\Windows\system32\RpcRtRemote.dll 0x2fb00000 - 0x2fb06000 C:\CDs\ccsv5\ccs_base\DebugServer\bin\LibraryLoader.dll 0x730c0000 - 0x73147000 C:\Windows\WinSxS\x86_microsoft.vc80.crt_1fc8b3b9a1e18e3b_8.0.50727.6195_none_d09154e044272b9a\MSVCP80.dll 0x72dc0000 - 0x72e5b000 C:\Windows\WinSxS\x86_microsoft.vc80.crt_1fc8b3b9a1e18e3b_8.0.50727.6195_none_d09154e044272b9a\MSVCR80.dll 0x2fc70000 - 0x2fe62000 C:\CDs\ccsv5\ccs_base\common\bin\xerces-c_2_5_0.dll 0x2fc30000 - 0x2fc53000 C:\CDs\ccsv5\ccs_base\common\bin\ti_logger.dll 0x2fe80000 - 0x2fef5000 C:\CDs\ccsv5\ccs_base\common\bin\C4DLL.DLL 0x30010000 - 0x30020000 C:\CDs\ccsv5\ccs_base\common\bin\CCReg.dll 0x30030000 - 0x30077000 C:\CDs\ccsv5\ccs_base\common\bin\fsutil.dll 0x30090000 - 0x30098000 C:\CDs\ccsv5\ccs_base\common\bin\fsutiljni.dll 0x300b0000 - 0x300ba000 C:\CDs\ccsv5\ccs_base\common\bin\MiniDump.dll 0x300d0000 - 0x30244000 C:\CDs\ccsv5\ccs_base\common\bin\setup_parser.dll 0x30260000 - 0x3026d000 C:\CDs\ccsv5\ccs_base\common\bin\ti_targetdb_parser.dll 0x71e70000 - 0x71efe000 C:\Windows\WinSxS\x86_microsoft.vc90.crt_1fc8b3b9a1e18e3b_9.0.30729.6161_none_50934f2ebcb7eb57\MSVCP90.dll 0x71dc0000 - 0x71e63000 C:\Windows\WinSxS\x86_microsoft.vc90.crt_1fc8b3b9a1e18e3b_9.0.30729.6161_none_50934f2ebcb7eb57\MSVCR90.dll 0x740d0000 - 0x740fe000 C:\Windows\system32\mlang.dll 0x74c10000 - 0x74c15000 C:\Windows\system32\msimg32.dll 0x75340000 - 0x754dd000 C:\Windows\syswow64\SETUPAPI.dll 0x765d0000 - 0x765e2000 C:\Windows\syswow64\DEVOBJ.dll 0x74e70000 - 0x74e91000 C:\Windows\system32\ntmarta.dll 0x756f0000 - 0x75735000 C:\Windows\syswow64\WLDAP32.dll 0x72f80000 - 0x72ff0000 C:\Windows\system32\ntshrui.dll 0x74790000 - 0x747a9000 C:\Windows\system32\srvcli.dll 0x74520000 - 0x7452b000 C:\Windows\system32\cscapi.dll 0x740b0000 - 0x740ba000 C:\Windows\system32\slc.dll 0x747b0000 - 0x747b9000 C:\Windows\system32\netutils.dll 0x73010000 - 0x7301c000 C:\Windows\system32\mssprxy.dll 0x340a0000 - 0x340f0000 C:\CDs\ccsv5\ccs_base\DebugServer\bin\ti_xpcom.dll 0x6f8e0000 - 0x6f9cb000 C:\Windows\system32\DBGHELP.DLL 0x36150000 - 0x362f0000 C:\CDs\ccsv5\ccs_base\DebugServer\bin\mdex.dll 0x747c0000 - 0x747d1000 C:\Windows\system32\NETAPI32.dll 0x74780000 - 0x7478f000 C:\Windows\system32\wkscli.dll 0x747e0000 - 0x747e7000 C:\Windows\system32\WSOCK32.dll 0x34150000 - 0x3416f000 C:\CDs\ccsv5\ccs_base\DebugServer\bin\XPCOMUtility.dll 0x363f0000 - 0x3666d000 C:\CDs\ccsv5\ccs_base\DebugServer\license\mdexutil.dll 0x740c0000 - 0x740c9000 C:\Windows\system32\snmpapi.dll 0x73380000 - 0x7338a000 C:\Windows\system32\wbem\wbemprox.dll 0x71d10000 - 0x71d6c000 C:\Windows\system32\wbemcomn.dll 0x76d90000 - 0x76dbd000 C:\Windows\syswow64\WINTRUST.dll 0x73370000 - 0x7337f000 C:\Windows\system32\wbem\wbemsvc.dll 0x71c70000 - 0x71d06000 C:\Windows\system32\wbem\fastprox.dll VM Arguments: jvm_args: -Dosgi.requiredJavaVersion=1.5 -Dosgi.instance.area.default=@user.home/workspace_v5_3 -Dorg.eclipse.equinox.http.jetty.customizer.class=com.ti.ccstudio.gui.composer.http.jetty.MaqettaJettyCustomizer -Xms40m -Xmx384m -XX:MaxPermSize=256M java_command: <unknown> Launcher Type: generic Environment Variables: PATH=C:\CDs\ccsv5\ccs_base\common\bin;C:\CDs\ccsv5\ccs_base\common\uscif;C:\CDs\ccsv5\ccs_base\DebugServer\license;C:/CDs/ccsv5/eclipse/jre/bin/client;C:/CDs/ccsv5/eclipse/jre/bin;C:/CDs/ccsv5/eclipse/jre/lib/i386;c:\Program Files (x86)\Intel\iCLS Client\;c:\Program Files\Intel\iCLS Client\;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\IPT;c:\Program Files (x86)\Hewlett-Packard\HP ProtectTools Security Manager\Bin\;C:\CDs\AltiumDesignerS09\System;;C:\CDs\ccsv5\eclipse;;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\.;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\../xmldb/aet_config;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\../xmldb/trace_config/setup;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\../xmldb/trace_config/devices;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\../../../common/bin;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\../../../common/uscif;C:\CDs\ccsv5\ccs_base\emulation\analysis\bin\../../tpi;C:\CDs\ccsv5\ccs_base\emulation\drivers USERNAME=Some User OS=Windows_NT PROCESSOR_IDENTIFIER=Intel64 Family 6 Model 58 Stepping 9, GenuineIntel --------------- S Y S T E M --------------- OS: Windows NT 6.1 Build 7601 Service Pack 1 CPU:total 8 (8 cores per cpu, 2 threads per core) family 6 model 10 stepping 9, cmov, cx8, fxsr, mmx, sse, sse2, sse3, ssse3, ht Memory: 4k page, physical 4194303k(4194303k free), swap 4194303k(4194303k free) vm_info: Java HotSpot(TM) Client VM (11.3-b02) for windows-x86 JRE (1.6.0_13-b03), built on Mar 9 2009 01:15:24 by "java_re" with MS VC++ 7.1 time: Thu Dec 13 14:45:54 2012 elapsed time: 19 seconds
If that give's any insight ...
Regards, Wolfgang
Thank you for tracking that down. Unfortunately, the java crash log didn't have anything useful. It is unusual that there is no .dmp file generated. The next thing that might help is the Debug Server Log. You basically enable the logging, recreate the crash, and collect the log file. The file will be big. If you are able to post that here we will see where that points.
Excuse, I didn't realise the dmp-file.
Also find attached the log file.6281.#DebugServer20121218074658.txt1768.#MyLog.txt
Wolfgang,
We had a look at this and believe the combination of emulators and devices is causing a problem. You're using a device that isn't officially supported by the XDS100v2.
What seems to be happening is there is a problem when the connect to the 2nd core is attempted. Whatever that issue is causes CCS to try to disconnect the 2nd core. The disconnect sends the software down a bad path and it crashes.
If you connect to the cores in the reverse order (2nd, then 1st), do either of the connects succeed?
Hello Andy,
There's no way (or as you called it only "bad paths") to successfully connect to the 2nd core. (Of course there's a way: CCS V3.3 & BH560 ;-)
Disregarding if I first connect the first core it crashes on the connect of the second or
if I directly connect to the second it crashes.
Are there good paths in the software leading to a connect to both ?
Regards, Wolfgang
Wolfgang,
I don't have a workaround for you. I have filed a defect against the C64x emulation driver (defect reference number: SDSCM00046041 ).
While the XDS100v2 you are using does not officially support this device, you are likely to encounter the same problem on other emulators.