Dear Sir:As well known, CC1020 or CC1120 can not be applied on SimpliciTI net provided by TI . But the advantage radio performance of CC1120 is very charming.I wonder that can I do some programming to realize requirement of SimpliciTI's the physical radio lay (MRFI) for CC1120? If possible? Please give some suggestion or key point on this work, if it is impossible? Give me some reason.
Thanks for your help !
Nelson
We are currently working on code for official support of the CC1120 in SimpliciTI. It is expected to be released around the beginning of December 2011.
As you indicate, there is no current support for the CC1020 nor are there currently any plans to support it in SimpliciTI.
Jim Noxon
If this post has answered your question, even if not the way you wanted, please indicate so by clicking the Verify Answer button on this post.Please start a new thread if your question is not closely aligned with the original post in this thread as it makes searches more effective.If responding to a post please click the Reply button on the post you are responding to rather than merely defaulting to the bottom post.
Dear Jim Noxon:
This is a good news for us.
We know what we should do in next a few month is that we will go on the current work base on CC1110 or CC1101 and prepare the CC1120 module .
Thanks.
Nelson Nee
Dear Jim Noxon:
Happy new to you. What is your work status on CC1120 supporting for SimpliciTI? My corp and I is waiting for your work. Would you like to tell me some information on this program?
Hello Sir.
I am Wayne.
I need SimplicTI for CC1120 too. When can I get the solution?
Please let me know the information.
Thank you.
The simpliciTI supporting CC1120(or CC1121) has released or not? If released, Where to get it? Thank!
Today is June 30,2012, which is far from "around the beginning of December 2011", can we use the offcial version for cc1120 driver for SIMPLICITI?
The simpliciTI supporting CC1120(or CC1121) has released or not? If released, Where to get it? Waiting for your kind reply. Upto It, we will decide on choice between CC1120 and CC1101.Thank!
Hello,
I post here in the hope that someone can finally answer to us...
Is there any chance to get MRFI or SimpliciTI ported for the CC1120/CC1125?We plan to use the new CC1125 so i need information....
Thank you in advance for your help.
Max.
The simpliciTI supporting CC1120 has released or not? If released, Where to get it? Thank!
Shijo
Are there any new to use cc1125 with simplicity?
Thank You very much.
Ismail