This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can CC debugger be resurrected by SmartRF 04 ?



Dear all,

I know cc debugger can be resurrected by SmartRF 05  (SWRU197.PDF PAGE 13) , how about SmartRF 04?

Thanks,

Dexter

  • Yes, you can also use SmartRF04EB. The procedure is EXACTLY the same. That means that you still need to select "SmartRF05EB" as the device in the flash programmer, as explained in step 2 on page 14 in the manual (the device is the device you are writing the bootloader to, and the flash programmer treats the CC Debugger and SmartRF05EB similarly).

    When connecting the SmartRF04EB to the debugger, remeber that the recommended way is to connect it via the SoC Debug Plug-in (SOC_DEM) board and not directly via P14.