Hi,
In CC1101 user manual, it is stated that "The frequency synthesizer must be calibrated regularly."
I am currently using Manual calibartion for a 2 way communication peer-to-peer devices. Hence, prefer to use manual calibration to maximise the RX time. During testing, it is observed sometimes, a device suddenly unable to receive any messages and the messages it send is not able to be received by others for a certain duration (no TX underflow/Rx overflow as I do a regular check on it). It self recovered after sometimes. Hence, I am suspecting it might be due to the RF out of syn.
Is there a maximum allowed in-between callibration time for CC1101? Is there any guideline that tell us how frequent do we need to calibrate?
Thank you.
Seng Kee