This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC-6LowPAN Edge Router OMAP-L138 Booting Error



Hi,

I got a CC-6LowPAN-DK-868 kit. I followed the quick Start Guide, connected CC1180EM on Adapter card on the edge router. insert the SD card and power on the Edge router. 

I got an error message at serial terminal like that.

Booting with TI UBL
Device OPP (300MHz, 1.2V)SD/MMC Boot failed.

 The red and green two LED in the CC1180EM adatpter card toggled on and off every 4 seconds. I know the linux kernel is loaded from the SD card.

Can someone provide links to replace the image in SD card.

Thanks in advance!

zy