We are developing a apparatus using CC1120.
Although we read specifications, we were not able to understand the right AFC setup.
Does the AFC operate for CC1120 correctly by the following register setup?
FREQOFF_CFG.foc_en= 1 (ON)
FREQOFF_CFG.foc_cfg = 11
(FOC in Frequency Synthesizer Enabled, Loop Gain factor 1/128 .)
But I wonder that we do not command "SAFC strobe".
Do we need to do "SAFC strobe" command with the FREQOFF_CFG setting ?
If we should command "SAFC strobe" , do we need to set the "SAFC strobe" in the act of receiving the preamble signal?
When is the best timeing of SAFC strobe?
Thanks.