Hi,
I have two pcs of Smartf05 EB ver 1.8.1. One of these evaluation board is not getting recognized by windows devicemanager as well as SmartRF Studio software. Following are strange observations that I have from the malfunctioning eval board.
1. If I keep the joystick button pressed down and power off and on the EB then typically the board used to display its MAC address however currently it only displays "TexasInstrument Smartf05 EB CC2530"
2. It's USB LED D6 continuesly glows whereas LED1, LED2, LED3 and LED4 typically remain inactive
3. If I Power Off/On the board few times then LED3 glows followed by LED2 and then LED1 i.e. all these 3 LED glow and LED D6 doesn't glow and there is no text displayed on the LCD.
4. I tried Forced boot recovery mode (as suggested in SmartRF05 Evaluation Board User’s Guide Swru210a.pdf) however LED D6 never blinks.
Please help suggest how to recover this eval board?
THanks
Anubhav