Hello all,
I have a file that I can program using the SmartRFProg application just fine, and set my IEEE address.
Now I am trying to use it on a command line to flash the file and set the IEEE address, and it is telling me the file is too big.
Does anyone know how to fix this? in the GUI app its two steps to program then set the address, I am ok with splitting it into two commands, but I cant find a way to make the command line set just the address.
Programming without setting the address through the command line works fine, programming and reading the address works fine, just programming and writing the address is a problem.
Command line output:
C:\Program Files\Texas Instruments\SmartRF Tools\Flash Programmer\bin>SmartRFProgConsole.exe S EPV F="out.hex" WI(F=0,I=AA.BB.FF.FF.00.11)
Texas Instruments SmartRF Flash Programmer v1.13.5-no-mfc
----------------------------------------------------------------------------------------------------
6902: Modifying flash image with IEEE MAC addr...
6902: Erasing entire flash...
6902: Programming flash....
6902: HEX file content at address 0x3FFEF exceeds chip's 128kB flash size