This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tiwi-sl initialization blocks



Hello

I'm setting up tiwi-sl with an stm32 controller

The spi code is based on CC3000 + MSP430 FRAM Basic Wifi Application/ spi.c 

wlan_start(0) function call is blocking on 

SimpleLinkWaitEvent(HCI_CMND_SIMPLE_LINK_START, 0);

(within SimpleLink_Init_Start)

The hci_command_send on the previous line seems to be going ok with command data going to tiwi-sl through spi

The interrupt on spi_irq fires but the received data is not a HCI_TYPE_EVNT, so hci_event_handler never finishes