Hi,
May I ask if the C2000 series MCU support 5V TTL input or not? if not, any recommended solution can be suggested?
Thanks and regards,
Barry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
May I ask if the C2000 series MCU support 5V TTL input or not? if not, any recommended solution can be suggested?
Thanks and regards,
Barry
Hello Barry!
You need the level voltage converter for this task. For example like this http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/137803.aspx.
Regards,
Igor
Govind,
I strongly recommend that you make the layout change. Measuring 4.7 V at the GPIO is outside of the Absolute Maximum Rating. You are at risk of damaging the device and impacting the reliability of the device.
Please see Tables 4.1 Absolute Maximum Ratings and 4.2 Recommended Operating Conditions in your Datasheet for more information.
-Mark