Hi,
I got the following error messages:
warning #10247-D: creating output section ".sysmem" without a SECTIONS
specification
"I:/workspace/sw/ide/ccs/cmd/f2806x/f28069M_ram_lnk.cmd", line 119: error #10099-D:
program will not fit into available memory. run placement with
alignment/blocking fails for section ".ebss" size 0xbcf page 0. Available
memory ranges:
RAML0_L7 size: 0xa000 unused: 0x328 max hole: 0x328
"I:/workspace/sw/ide/ccs/cmd/f2806x/f28069M_ram_lnk.cmd", line 120: error #10099-D:
program will not fit into available memory. placement with
alignment/blocking fails for section ".econst" size 0x573 page 0. Available
memory ranges:
RAML0_L7 size: 0xa000 unused: 0x328 max hole: 0x328
error #10010: errors encountered during linking; "Servodriver.out" not built
And this is in the f28069M_ram_lnk.cmd file:
.ebss : > RAML0_L7, PAGE = 0
.econst : > RAML0_L7, PAGE = 0
I case of RTFM , which one?