This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280041: F28004x for IEC60730/UL1998 functional safety

Part Number: TMS320F280041


Dear Champs,

I am asking this for our customer.

They used to use F2803x for IEC60730/UL1998 with the software library and certificate we provided.

Now, they are thinking to use F28004x like F280041.

Do we have corresponding software library and certificate with F28004x like we did with F2803x?

In 

http://www.ti.com/microcontrollers/c2000-real-time-control-mcus/overview.html#safety

it says F28004x can support up to IEC60730 class C.

Would you please show us the related software library and certificate explicitly?

Wayne Huang

Would you please show us the software collaterals

  • Hi Wayne, 

    Support for F28004x is currently work in progress.  We do not have the certification yet, but we do have an Alpha release available via mySecure.  The Alpha intended for early adopters and can be used for proof of concept purposes.

    Also F28004x is IEC60730 Class C capable.  Please note that while we are planning to get ISO26262 ASIL B certification for a subset of the overall solution, we are not planning IEC60730 certification. 

    Please send us an email and we can provide you with all the details. 

    Cheers! Krishna