Hi,
I have a problem using the On Chip Flash utility in CCS 4.2.3 when trying to write the flash in a Piccolo device via an XDS100. If I make a configuration file with one XDS100 connected to a Piccolo, it works fine. Howvever, if I make another configuration file with two XDS100's, identified using the serial numbers, with the second XDS100 connected to a OMAPL138, then try to write the flash in the Piccolo I get errors:
C28xx: Flash Programmer: Missing Flash Programming Settings.
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Missing Flash operation option. Operation cancelled.
C28xx: Trouble Writing Memory Block at 0x3f4000 on Page 0 of Length 0x916
Cannot write to target
When I look on the 'On-Chip Flash properties form I see a single message 'Property for node name 'FlashProgrammerNode' could not be found in 'PropertiesDB.xml'
Any ideas?
Cheers,
John.