The project I'm currently working uses the enet_uip_m3 as the base for the ethernet comms and everything is working fine.
The problem is: this example uses the F28M25x_generic_M3_RAM.cmd and F28M25x_generic_M3_FLASH.cmd linker files and neither of those uses the shared Sx memory, and my project will be using it. But if I try to add those areas, the ethernet stops working.
I'm assuming that, although not shown on the linker file, uDMA configured on enet_uip_m3 is using that area to process it's stuff and thou, conflicting with the rest of my code.
So my questions are:
is my assumption correct? how to I check which areas the uDMA is using?
thanks.