This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Exporting Data in CSv4



Hello,

 

I'm capturing A/D data and graphing it in CSv4.  Is it possible to export the data to a file?  I am using Sci-Lab for algorithm testing and would love to use that data.

I tried the exporting data option but that does not seem to work. 

Thank you,

Jon

  • You can export data from the memory map. Set the address to the buffer you used for the graph, choose the data format, hex, binary etc and then click on the green chip with the arrow; in the drop down menu choose save and then save it to memory in a .dat file (you need to specify how many bytes to save) in the format you want. If you want to use the data directly you might need to go into the .dat file and delete the top line which has a bunch of header info