This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3050 will not enable charge until SMBus activity

Other Parts Discussed in Thread: BQ3050

I have a BQ3050 implementation using four Li-Ion cells. I connect the battery pack to a charger and the BQ3050 will not turn on the charge FET. I found that if I connect the EV2300 pod to the pack for just a second, the charge FET is turned on and everything works from there. If I disconnect the battery from the charger and then reconnect within 10 seconds, charging occurs as expected. If I disconnect for a longer time and then reconnect, it will not charge. Then I found that just tapping either SMBus line with a scope probe will enable the charging. Are pull-ups on the SMBus lines required for charging? I do have them on the system in which the pack gets installed but not on the stand alone charger and not in the pack itself. I have the 200 ohm/100pF/100 ohm network as in reference schematic on each line.