This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'd like to use TI's LM5001 (Non-Automotive Version) for our IP PBX application.
Specification
- Vin: 48V
- Vout: -26V, -42V, -58V
- Iout: Max 0.7A (700mA)
1) Power Topologies
• Supply power to SLTC in PBX using CUK Or Inverter charge pump
2) TI Part
• Design of Negative Output and Multi port using LM5001
-. By changing the Buck Converter, the negative output state is created, and then the output voltage is synchronized to supply the load share and output with -11.6V, -23.2V, 34.8V, -46.4V, -58V.
• Competitors are: Linear LT3758
3) Competition PBX Reference Power rail
4) LM5001 concept (Previous developer received from TI BU.)
5) Questions
-. Charge pump & COUT Value
-. FB stage of OP input value & Compensation Value
-. 6 Winding design guide
thanks,
TS
Hi TS,
For further information, please see application note: Using a buck converter in an inverting buck-boost topology (SLYT286).
Regards,
Tim
Hi,
In the document titled "Stacked-Cuk" previously sent by TI, the available "Transformer" type says "VPH3-0138-R".
The vendor of this part is "COPPER Bussmann". Please refer to this company's application note for the help of this document.
There is an example called "SLIC Power Supply" in the last page of the document below.
BUS_Elx_App_Notes_Versa_Pac_as_Flyback.pdf
So, thank you for your review.
TS
Hello TI,
Hello,
Below is a schematic designed by referring to Stacked-Cuk method sent from TI side.
It seems to be a lot of errors because it was drawed with low understanding of Stacked-Cuk.
The Op Amp. (LM258ADR) used in the schematic below is from the "Vcm include ground" property as shown in the Stacked-Cuk circuit diagram from TI.
So, please review the above schematic.
Regards,
TS