This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24070: Can VREF be used to pull input pins high?

Part Number: BQ24070


The ISET2, MODE, and CE pins have an absolute maximum voltage rating of 7 volts. The data sheet does not give an absolute maximum on input current. I want to pull those pins high but I don't know the best way to do that because the input voltage that I will be working with could on occasion go as high as 12 volts.

1.  Is it ok to use pin 1 (VREF) to pull pins 7, 8, and 9 high? Could they be tied directly to VREF or would a pull up resistor be required?

If I can't use VREF for the pull up voltage, then the following questions apply.

2.  If I connect any of the pins 7, 8, and 9 (ISET2, MODE, and CE) to a 100k resistor whose other terminal is tied to pin 4 (IN) and to 12 volts, will it cause a malfunction or damage to the part?

3.  Is it ok to tie pins 7, 8, and 9 together and then pull them all high using a single resistor to pin 4?

If that doesn't work, then my solution would likely be to use a 5.2 volt zener to limit the voltage. And that brings one more question.

4. Can pins 7, 8, and 9 be tied directly to a 5.2 volt zener limited source derived from the voltage at pin 4 (IN)?

  • Hello
    The VREF pin is specified as having a max output current of 20mA, so it could be used as a source to pull up the three pins in question.
    Recommend to use a 10k ohm resistor for each pin to prevent any possible cross talk or start up issues between the inputs.
    Current draw on ISET2 is listed as 40uA high while CE and MODE are about 1uA, 10k ohm pull up is a little safer than 100k.