This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: Output exceeding fixed value

Part Number: TPS61099


Hello,

We are noticing a strange phenomenon with the TPS610995. Vin=3 Vout=3.6 fixed

  1. If we startup the device with the 3V bench power supply without a current limit, the output comes up to 3.6V just fine.
  2. If we startup the device with the 3V bench power supply current limited (200mA), the supply hits the limit and the device outputs less than 3.6V
  3. If we start increasing the current limit, the device output voltage will rise up to 3.6V. However the bench supply is still hitting current limit.
  4. If we increase the current limit further until it no longer hits the limit, the output voltage of the device reaches 5.6V. However the current flow drops dramatically at this point.

I'm not sure how it's possible with the internal feedback resistors for this device to ever output greater than 3.6V.

Is there something with this current limit process that is putting the chip into a weird state?

Let me know if there is any other pieces of data you need.

Regards,
Ryan B