This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5023: LM5023 POWER SUPPLY, snubber Resistor heating,

Part Number: LM5023


Hi,

We are designing a LM5023 POWER SUPPLY, Here the snubber resistor is heating,

Find the attached schematic.

In schematic R3,R4 resistance value is 50K/2W, D2 is UF4007, Across R3,R4 parallel connected TVS diode 1.5KE200CA connected,

Mosfet and Secondary diode is no-heating,

Kindly suggest the appropriate snubber resistor value.

Input: 84V -264 Vac 

Output: 24Vdc, 4.2A

Transformer destails,

L= 239uH, Primary : 40T, Sec= 7T , Aux= 4T

     Regards,

Sathishkumar V