Hi, mi name is Andres Bonzani and this is my first post. I speak spanish and my english not is good.
I designed a battery charger using the IC: BQ24075
The schematic is this:
The PCB´s are there:
OK, the problem is when i put the power on mi circuit, the charge no start.
The rest of my circuit works fine.
The pin SYSOFF works fine when the power is not conected (I can drive de FET ok).
The two led´s works fine. When the power and battery are connected both are turned on. When the battery is removed CHG led is turn off.
By measuring the current flowing through the battery is 0mA.
The IC is good solder.
I´m confused
I'm doing wrong?
thanks