Hi
My application requires charge a SLA battery 12V / 40Ah from a Solar panel.
The charger should allow solar panel from 22W to 100W ( panel Optimun operating voltage (Vmp)= 17V )
i itend to use the next circuit, ( reference: doc SLVA437A )
vmppt set=17v vbat=14.59 v i charge=8A
My questions?
- what is the the charge current in a pre-conditioning mode ? 1/10 of fast charge? what is the time?
- Is possible reduce de Precharge region time in this circuit?
- What is the charge current when a voltage in the solar panel drops below the mppt set voltage (17V ) ? What is the Min voltage necessary in the Input, to charge the battery?
I await your observations and suggestions to optimize the circuit
Thanks
Regards