Hello,
we are using the SM72295 as a driver for a full bridge DC/DC converter. VCC is connected to 12V and VDD is connected to 5V and bypassed with 100nF as described in some application notes and the datasheet. (BTW: There is a mistake in the datasheet, VDD is listed as "output")
it happened now two times that there was a short circuit in the chip between VDD and AGND, one time it happened without there was any voltage on the HB and HS pins and no pulses on the input pins. So even in this mode, where the driver didn't do anything VDD broke though!
SIA, SOA, SIB and SOB are pulled down GND with 10kOhm, IIN, BIN, BOUT and IOUT are pulled up to 5V also with 10kOhm, because those amplifiers are not used.
Can you give me some adive here, how can I protect the SM72295 from breaking?
Best wishes
Johannes