1st post here.
I have been trying to get this kind of power supply running for a while but I could not get enough stable specifications until recently.
I have tried to get help from a couple of power supply chip manufacturers but did not get anywhere as everyone seem to
cater for off main supply.
=====================
Isolated input to output.
Input voltage: 35Vac-46Vac or wider
50 Hz (47-63 Hz preferred)
Output voltage: 50V 1.2A centre tapped (+25V 0 -25V)
Sine-wave current draw
Power factor between 0.9 capacitive and 0.95 inductive
Temperature range of -5°C to +60°C
=====================
Any hints, design notes ect. appreciated. The magnetics are a bit of a nightmare I guess. :(