• TI thinks resolved

DC/DC converter with adjustable output Voltage

Hello,

i am looking for an DC/DC Converter.

Inputvoltagerange from 24V to 36V

Outputvoltagerange from 4V to 23V

Outputcurrent from zero to 5 A

I need three of these Outputs in my circuit.

It would be great when we could monitor voltage an current from the output.

Many thanks for the support

Philipp