sir,
In our project we are using TLV1117-50CDCY we giving Vin=12V and taking Vout=5V . Its generating excess heat when we connected 250mA load .plz reply as earliest.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
sir,
In our project we are using TLV1117-50CDCY we giving Vin=12V and taking Vout=5V . Its generating excess heat when we connected 250mA load .plz reply as earliest.
Veeresh,
The power dissipated in the device is VIN*ICC+(VIN-VOUT)*IOUT = 12V*5mA+7V*250mA = 1.81Watt
The heat needs to flow easily into the printed circuit board then the PCB conducts heat to ambient air.
If the tlv1117 is too hot then the PCB is too hot or the PCB does not accept heat from the tlv1117 well.
There should be a good thermal path from the copper under the tlv1117 pad to the PCB ground plane.