Hi~
According to datasheet, an external diode is recommended for protecting TLV1117 if the input instantaneously is short to ground.
May I know what the minimum requirement for this diode? Is it okay to use 1N4148WS-F?
Thanks and Best regards,
Tiger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi~
According to datasheet, an external diode is recommended for protecting TLV1117 if the input instantaneously is short to ground.
May I know what the minimum requirement for this diode? Is it okay to use 1N4148WS-F?
Thanks and Best regards,
Tiger
Hello Tiger,
The note and the diode chosen are for general guidance.
I can't say for sure that there is a minimum specification for the diode, just that it will depend on the application.
I am sure that you're aware that 1N4002 can handle more surge current than the 1N4148, so I would say that if the application doesn't exceed the specification of the 1N4148 when the input is shorted to ground, then using the 1N4148 should be acceptable.
Best,
Michael