hi ?
My customer got a problem with eth TPS62110 . ( production STOP). The output voltage is 0V when the input voltage is 6V. He observe in this case that the Iout is 200 mA .
He doesn t know how it is possible to have it ( the input votage is < 17V ).
When he switch off the Vin et switch on again , the Vout is correct .
The Vin max in the system is 16 V .
The Vsync is driven by a MCU . In the application , this pin is used to force teh PWM mode ( sync =1) with a frequency of1 hz for a time of 10ms .
the main time the sync pin is 0.
could you help us for this case ?
thanks
mickael