Hello,
I had a previous version of my board I used the TPS63031 with power save mode disabled (PS/SYNC pin wired to VIN). The output voltage was perfectly regulated to 3.3 V. In a new version of the same board, I kept the same basic circuit and changed only the power save mode to enabled by wiring PS/SYNC to ground.
Now, with essentially no load (I estimate at most 10 mA) I'm seeing voltages slightly above 4.0 V in the output. Connecting a 20 ohm resistor to the output lowers the voltage to 3.6 V, which is still far away from 3.3 V even with a somewhat significant load. I tried using 1 uH and 10 uH inductors with no effect in output voltage in the no-load case. The input voltage is about 4.2 V if it matters. I measured the output voltage with an oscilloscope and I see very little ripple, a few tens of mV at most. I'm using about 120u of input capacitance and 20u of output capacitance, all routed close to the IC in the PCB (the same as I used in the previous version of my board where regulation was fine).
I did read in the datasheet that in power save mode the voltage may be above nominal, but I was not expecting it to be off by so much. Plus even if it were, I'd expect to see significant ripple. The TPS63001 datasheet, which as I understand is the same component but with a beefier switch, shows output voltage graphs in power save mode which show a 100 mV ripple, a situation quite unlike what I'm seeing.
So, should I search for a mistake somewhere else in my circuit or the PCB, or can the regulation in power save mode indeed be off by that much.
Thanks
Décio