Hello!
I have a project for the input range 60 V max. DC & output 8.4V , for this purpose I selected LM-5010A IC. I prepared schematic using webench designer. In this the system do not grounded the RTN pin , although I checked in datasheet it is been grounded for internal circuitry. Kindly tell me whether it is intentionally not grounded or it is system error. I attached also the design.6371.8.4V Circuit.pdf
Regards,
Mohit Chopra