Hello:
I'm designing a 500V to 15V, 0.75W flyback converter using the TPS40210.
Because the input voltage is high and the power is low, the current going into the switching MOSFET's drain is small, and the current coming out of the source is significantly influenced by the gate current.
As a result, I'm getting a rather large square wave imposed onto my current waveform. Because the square wave is so big, I can't really filter this out with a simple RC filter, so I have to rely on the leading edge blanking in the TPS40210 to ignore it.
My problem is the pulse is around 170ns and the datasheet gives a typical blank time of 75ns. I tried lowering the gate resistor, to drive the MOSFET faster (IRFBF20) but it didn't seem to help much. I suppose I could find a lower gate charge mosfet (IRFBF20 is 38nC) or a faster one, but I'm already a little worried about putting too fast of an edge on such a large voltage.
Does anyone know a good way to deal with this problem? Is this really a problem? The circuit seems to work in the simulator but I'm worried that when I build it, it will be erratic because it may respond to the hump at lower current commands and to the end of the ramp at larger current commands.
I attached some waveforms from my simulation. The red is the voltage at the sense resistor, and the green is at the ISNS pin after my RC (499-ohm, 75pF). The hump is around 170ns wide.