TPS65950 can only supply 100mA current on VBUS, but we need more current supply to our USB OTG port. On page 23 in the User's Guide of 65950(SWCU056C), it mentioned that "In case there is a need to use an external 5-V supply for larger current needs then one can use an external supply; however, the VBUS pin from the device must be connected to the VBUS pad on the USB connector." So my question is how to design a circuit to implentment the notes mentioned. Can I just connnet a external 5V power supply to the VBUS net betweent the USB connector and TPS65950?