I have a prototype with the bq51013 in the YFF package. I followed the layout guidelines as shown in the documentation for the BQ51013EVM-725 - Evaluation Module for bq51013
There are six pads that required vias and I took my best shot at the layout. We are struggling with putting the bq51013 YFF package down on the first board as it looks like the board house grew the pads with the vias. I should have asked this before having the board fabbed, so here are my PCB layout questions:
1) What is the recommended pad size for the YFF package? (I used 0.20 mm which is approx. 8 mil for 1oz copper pcb)
2) What is the recommended via and hole size for the 6 signals that need routing from the center of the part? (I used 0.228 mm/ 9 mil via with 5 mil hole size)
3) What is the recommended finish for the PCB? Can you have a leaded (non-ROHS) finish?
4) The ball material under the column "Lead/Ball Finish" says 'Call TI' in the device data sheet under Package Option Addendum. Which phone number?
5) What is the melting temperature of the ball material? Is there a recommended temperature (we are guessing 255 C)?
Thanks,
Thom