Hi,
I have built several boards using the bq51013 EVM receiver circuit and a TPS61085 boost converter circuit(designed in SwitcherPRO Design Software) to increase the voltage level to 5.7Volts. The problem that is that when a load of 580mA(required by end application of the circuit) is connected the system begins to restart again and again and continues as long as the load is attached. the boost converter draws 780mA of current during this state.
At a lesser load of about 350mA at boost converter output the system works just fine.
What could be the possible reason for the circuit for not being able to deliver the required load current. And how can it be fixed. Schematic of the circuit(W C R.jpg) has been attached for reference.
Thanks,
Hyder