This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Can MMWAVE-DEMO-VISUALIZER support load configuration but not send to device

Part Number: AWR1642


Hi,

My customer is using the SDK 1.0.0.5, now they can run the mmw demo well. We tried to fix parameters for test, why not send configuration from PC, but still want to display the result in MMWAVE-DEMO-VISUALIZER. Currently the demo can run well with fixed parameters, and data can be received in the PC through terminal. But the plot cannot displayed on the MMWAVE-DEMO-VISUALIZER. I think it is need to load configuration into MMWAVE-DEMO-VISUALIZER for display, but I don't find one button in the visualizer. Would u pls help change it to support configuration load only?

In the previous SDK 0.8, the demo run is through command, and it can support load configuration only. 

BR,

Andy