The AWR1243 datasheet specifies the device uses a 40 MHz clock as the local oscillator. It states, and responses to others' questions have confirmed, that that clock can be shared/cascaded to other devices. Elsewhere, the datasheet also specifies –91 dBc/Hz (77 to 81 GHz) of phase noise at 1 MHz.
My questions are as follows:
(1) What does the phase noise look like at frequencies closer to the carrier?
(2) Are the 40 MHz LO or 20 GHz RF synthesizer the primary source of this phase noise? I.e., if fed by an external device with better phase noise can the system's phase noise be improved from the -91 dBc/Hz value from above?
(3) Is there any meaningful limit to how many devices can be cascaded if an external clock or synthesizer are used?