Other Parts Discussed in Thread: IWR1443
I'm performing some Radar Studio evaluation with the IWR1443 -> mmWave DevPack -> TSW1400 hardware chain and have gotten to the point where I am able to fully configure the system.
However I have questions about the document here
Q1:It said that total period of data capture (=frame periodicity x No. of frames) < 10 seconds,what dose that mean?
I have collected some data successfully by using this setting in radar studio ,using one TX and four RX channels.I can get the data file, its size is 204800KB.
Different from the documentation, the total signal time here is 100 seconds(My frame periodicity is 1s and the number of frames is 100, giving a transmission time of 100s), well over 10 seconds. In operation, I first click "TSW1400 Arm" until the output interface displays "[RadarAPI]: TSW1400 capture complete" before clicking Trigger Frame, and then click "TSW1400 Arm" to save the data to the computer.
Q2: Is this correct? So I can not care about the total signal time, as long as the amount of data within 1GByte (TSW1400 storage ceiling) ?