A few months back, I ordered a couple Stellaris Launchpads, only to find they were out of stock after I ordered. Over a month later, the back ordered devices came in and I've been very excited to dive in. I currently have an MSP430 based design that I have been hoping to migrate over to the Stellaris due to the extra processing power.
However, when I downloaded the whole StellarisWare and accompanying CCS v5.2, I have problems. For starters, during the CCS installation, the progress box that lists what files are being installed/actions being taken/etc. will repeatedly say "Installation Failed" for at least 10 lines, then it goes back to installing other things. After a while of installing, it will, again, repeatedly say "Installation Failed". However, the final installation finishes and gives me the option to launch CCS, which I do.
Once inside I launch, what seems to be, CCS, I'm greeted with the Eclipse splash screen with no reference to CCS. In the editor, again, there is no reference to CCS and the options to open a project is grayed out... What gives?
One final note... Am I NOT going to be able to use CCS with the Stellaris, except for a 30-day trial? I'm a student and I can't afford a $500 license just to play around with a $15 Launchpad...