Hi,
I'm using the Zigbee ZStack-CC2530-2.3.0-1.4.0 with IAR workbench 8051 and SmartRF Flash Programmer to program a module CC2530F2530.
I want to upload a sample hex file came from the installation CD into the device, but it says "Could not open specified hex file".
I have tried many of the sample hex files, but none of them works. The interesting thing is that my friend successfully uploads a hex file into the same device and he passes the device to me. I can use "read flash into hex file" to download the program from the device into a hex file and then use "erase, program and verify" to upload the same hex to the device. But I can not upload any new hex file to the device. Any help is appreciated!