This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: Debug problem using ULink Pro ...

Part Number: CC2538


I am using ULink Pro to debug an CC2538 custom board. The debug connection is implemented through an 6 pin Tag-Connect header. The signals are connected according the data sheet of the CC2538 and ULink Pro. Here are the connections:

CC2538 ---> ULink Pro (J1 device internal)


- JTAG_TMS pin 46 ---> TMS_SWDIO pin 2
- JTAG_TCK pin 47 ---> TCL_SWCLK pin 4
- JTAG_TDO pin 48 ---> TDO_SWO_TRACE_CTL pin 6
- VCC ---> VTREF pin 1
- GND ---> GND pins 3, 5, ...
- /RESET pin 28 ---> nRESET pin 10 (through 1k in series and 10k pull up)

I have verified the connections and they are correct. I do see the clock on TCL_SWCLK pin 4 in ULink Pro and I do see outgoing data traffic on TMS_SWDIO pin 2. There is no data traffic coming from the CC2538 side. I can program the CC2538 through its built-in boot loader, the hardware is working.

The ULink Pro is set to SWD mode, the connected chip is not recognized.

What do I miss here? Any help is appreciated. Thank you.