Hi,
I want to use WL1837 chip as Host AP with 5GHz frequency band.
To set the mode 802.11a, in hostapd.conf set hw_mode=a,put the channel number 149.
Any other configuration required to change for setting up 802.11a mode ? If yes then please tell me parameters to set with which values.
802.11n mode in 5GHz :
And for setting up 802.11n mode, set ieee80211n=1 in hostapd.conf.
For that can you please suggest me which more parameters needs to be set and with which value.
Channel number that will work in 802.11n 5GHz mode ?
Also please suggest more option that enhance the performance.
Thanks in advance for help.