Hi,
We are working on a RSSI Measure Project using cc2540 in the Central Role.The detailed information is as follows:
1) BLE 1.4 stack
2) using cc2540 in the Central Role
3) using ipod in the peripheral Role
It began to read rssi value using "SimpleCentralRssiCB" func, but I found that the rssi value no change. When the data reading and writing will be updated. There is no constant RSSI update if there is no data packet tranmission.
Would like to understand that if the BLE1.4 stack is still with the issue of not having the RSSI update while in IDLE mode (no data packet transmission).
Thanks.
Regards,
Eric