Hello everybody,
I am wrestling with this device for quite some time now. I have a CC3000 module with the driver version 1.7.2.2. I want to update this driver because some other things are not working correctly under te older version. So I hope to solve some issues with the 1.14 version.
I downloaded the MSP430 flash tool, according to page 11 from
https://www.grc.com/dev/tqc/AdjustableTrebleShooter-v1.2/MSP430_Flash_Writer/MSP430Flasher_Doc.pdf
I connected the CC3000 board to my PC. Windows 7 automatically installed the driver. I can see now the MSP430 Application Uart as a COM Port. If I invoke the command:
MSP430Flasher.exe -n MSP430FR5739 -w PatchFlasherDriver.txt
The file is transmitted correctly.
But according to page 12 of the Flasher Doc I can also read the invoked File. But if I do so, after I transmit the PatchFlasherDriver.txt I am getting different Values.
For Example: The PatchFlasherDriver.txt starts with:
@c400
02 00 00 1C 7C 1B 01 00 03 1C FF 00 01 00 04 1C
When I read the output.txt file I am getting:
@C200
02 00 00 00 09 04 08 00 05 00 00 00 00 00 FF FF
Why is that happening???? If I read the firmware version through basic_wifi_application I am still getting the old driver version...
I appreciate any ideas..
regards,
F.S.