I'm working on implementing a receiver using a CC2541 for an existing transmitter that uses a CC2511 with the following parameters:
TX Freq's: 2,424,999,887 Hz, 2,449,993,677 Hz, 2,474,737,539 Hz, and 2477236919 Hz
Bandwidth: 334.7 kHz
Modulation: MSK
Data Rate: 49.987 kbps
Is it possible to set the CC2541 to a data rate that low? Table 25-10 in the CC2541 user guide leads me to believe that only 250, 500, 1000, and 2000 kbps are supported. Am I missing something?