I have been trying to my code to connect to an AP but after much debugging and thinking it was the exra code added in I see the code is in fact hanging at establishConnectionWithAP(); is there something I am missing in my code. Any help would be appreciated.
Thanks
Kas
P.S. My full code (ll functions can be found in this post but the "main" that I am using is included below
/*
* Application's entry point
*/
int main(void)
{
INT32 retVal = -1;
retVal = initializeAppVariables();
ASSERT_ON_ERROR(__LINE__, retVal);
/* Stop WDT and initialize the system-clock of the MCU
These functions needs to be implemented in PAL */
stopWDT();
initClk();
/* Configure command line interface */
CLI_Configure();
CLI_Write("\r\n\r\n\r\n\r\n\r\n\r\n");
//Initialise I2C
// I2CInit();
//Initialise I2C
// mpl3115aInit();
displayBanner();
/*
* Following function configures the device to default state by cleaning
* the persistent settings stored in NVMEM (viz. connection profiles &
* policies, power policy etc)
*
* Applications may choose to skip this step if the developer is sure
* that the device is in its default state at start of application
*
* Note that all profiles and persistent settings that were done on the
* device will be lost
*/
retVal = configureSimpleLinkToDefaultState();
if(retVal < 0)
{
if (DEVICE_NOT_IN_STATION_MODE == retVal)
{
CLI_Write(" Failed to configure the device in its default state \n\r");
}
LOOP_FOREVER(__LINE__);
}
CLI_Write(" Device is configured in default state \n\r");
/*
* Assumption is that the device is configured in station mode already
* and it is in its default state
*/
/* Initializing the CC3100 device */
retVal = sl_Start(0, 0, 0);
if ((retVal < 0) ||
(ROLE_STA != retVal) )
{
CLI_Write(" Failed to start the device \n\r");
LOOP_FOREVER(__LINE__);
}
CLI_Write(" Device started as STATION \n\r");
CLI_Write(" Location C \n\r");
/* Connecting to WLAN AP - Set with static parameters defined at the top
After this call we will be connected and have IP address */
retVal = establishConnectionWithAP();
if(retVal < 0)
{
CLI_Write(" Failed to establish connection w/ an AP \n\r");
LOOP_FOREVER(__LINE__);
}
CLI_Write(" Connection established w/ AP and IP is acquired \n\r");
CLI_Write(" Location D \n\r");
/*Before proceeding, please make sure to have a server waiting on PORT_NUM*/