I have a few CC1350STK (SensorTags) (Rev. 1.4.5 and FW Rev 1.3.1) and SensorTag DevPack. I want to try the three configurations a) Role Switching, b) Beacons and c) Concurrent. My questions are related to this.
1) Is the Firmware to try the above configurations included in the shipped product (with the above listed FW Rev.)? If yes, how do I enable these configurations? Currently only BLE stack seems to be active.
2) If the shipped Firmware does not include these features, where do I find the required firmware and how do I flash it into the SensorTag?
3) As per TI's documentation: "TIDEP0084– November 2016 TIDEP0084: Sub-1 GHz Sensor to Cloud Industrial Internet of Things (IoT) Gateway Reference Design", I tried to flash the file "sensor_cc13x0stk.hex" into one of the SensorTags using DevPack. But, the SmartRF Flash Programmer 2 gave the error: "Invalid checksum on hex record with address: 0xFFFF" for the file and also made my SensorTag dead. How do I restore the working firmware into the SensorTag?
4) The instruction sheet enclosed with the product refers to dev.ti.com/CC1350STK. But this page does not seem to exist. Is there a different location for documentation? Even after extensive searching TI sites, I could not find sufficient documentation for CC1350STK. Can you point me to the right url(s)?
Thanks in advance for your prompt reply.