Part Number: TCAN1042H
Hi
Is this part could achieve CAN in and CAN out, if no, any idea for that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Red,
The TCAN1042 takes an MCU I/O (TXD and RXD) and converts it to the CAN bus signals. It is possible to contruct a CAN repeater (CAN bus in, CAN bus out) using two CAN transceivers. However, external logic control is needed in order to ensure that the CAN buses do not enter a permanently dominant state.
Please feel free to email me separately for more information on a CAN repeater design.
Best Regards,
Max Megee